Part Number: AM26LS31
Hello,
Our customer use the AM26LS31,using with transceiver IC (SN75176).
The customer connect the AM26LS31 and the SN75176.
When power on, the driver of the SN75176 output high level for a while.
So, the low state output terminal of the AM26LS31 is damaged.
The DS26LS31 has short circuit protection.
Can the DS26LS31 avoid a damage as described above?
I thought the protection effective for only output short (Y and Z)......
Best Regards,
Naoki Aoyama