This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8041: How can I power off this HUB by receive a signal?

Part Number: TUSB8041


Hi TI Team:

I need to power off the HUB by receive a signal sent by CPU ,such as ClearPortFeature(Port_Power) ,how can I achieve this function?

  • Hi Henry,

    The TUSB8041 is a self-powered hub, so it cannot be entirely powered off by a USB command. It can be put into low power mode by the USB host if both the USB 2.0 and USB 3.0 buses are put in suspend / U3. Also, the hub's downstream ports can be powered off by the a command from the USB host as you noted above.

    Regards,
    JMMN