This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65982: Quick PDO change like EVM default FW

Part Number: TPS65982

Hi Team,

My customer is facing hard reset loop issue in Interconnectivity test using released Type-C PD peripherals(Their product is always working as source). According to the engineer, one product seems to draw more current than the value determined by PDO communication. Due to that over current condition, the Source issues hard reset and that is repeated.

Alt mode feature is more important than Power supply function, so they would like TPS65982 to switch to a Source that has only 5 V 0 A PDO.

Do you have any idea to realize their request?

I'm wondering if we can utilize FW setting implementing in default FW and GPIO controls after hard reset condition.  

Regards,

Takashi Onawa