This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB4041I: USB Hub not enumerating ever; Unknown USB Device Descriptor Request Failed or device descriptor read/64 error 071

Part Number: TUSB4041I

Hi,

Made what I thought was a pretty basic TUSB4041I circuit, with optional I2C connection to a microcontroller. All power rails are good, look clean, resets are at great levels, but device does not enumerate.

In Windows 10, I see the hub as an Unkown USB Device (Device Descriptor Request Failed), VID/PID are 0x0000 and 0x0002.

Under Linux, dmesg shows:

> new full-speed USB device number 7 using xhci_hcd

> device descriptor read/64, error -71

and then it goes through device 8, 9, and 10, all with same error -71.

So, please take a quick glance at schematic. Probably did something dumb.

Thanks.

> device not accepting address 9, error -71