Part Number: SN65HVD3082E
Other Parts Discussed in Thread: SN65LBC184
Hi Team,
Here is south China FAE Sunny, we meet a SN65HVD3082E communication problem, customer use SN65HVD3082E communicate with USB 485 debuger, the wire is only 1 meter, the SN65HVD3082E is on a circuit board which powered by isolated AC/DC power module(isolated from the ground of 220V power line), and the USB debuger is connect to PC, and PC`s GND is connect to ground to of 220V power line.
we found that SN65HVD3082E output lots of noise even USB 485 debuger don`t send any data:
But SN65LBC184 and SP483(local brand 485 device) can work good at this condition, customer are using SP483 currently, we want to use SN65HVD3082E to replace it, but it meet this problem, SN65LBC184 can work, but price is too high.
Could you help to give some comments on why SN65HVD3082E meet this problem while SN65LBC184 not?
Thanks very much.
Regards, Sunny