Part Number: DP83620
Hi all,
I am trying to make sure that the DP83620 can be used as a media converter from an RJ 45 with magnetics. I think it is capable of output NRZI or NRZ also known as PECL output or FX output to drive an LED but I need to make sure. Essentially I am hoping it can connect from an RJ 45 and act as the PHY layer which can be used as an optical media converter, and receiver of an FX electrical signal from a photodiode and maintain the auto negotiation for the different 10 mb/s and 100 mb/s. Does there have to be software embedded on to this device? Would there be FX output be able to modulate an LED if I amplified it (in theory)? Would the connections to the RX signal be differential from or can it take a direct signal from a photodiode?
After I get out a FX signal the signal needs to be amplified to drive a high power LED. The FX signal would come out at what current and voltage? Can i use something like a wide band transconductance amplifier (OPA 861) and a high speed high power mosfet capable of ~32 mhz at ~600-750 ma and 11.2 V to modulate the LED?
Can I use something like the OPA 694 to receive the photodiode and then into High Speed Differential Driver such as the analog's AD8131 or some TI equivalent.
I realize there are several questions in this thread, the main priority is the function of the DP 83620.