Part Number: TCA9548A
Other Parts Discussed in Thread: USB2ANY,
I have used TI USB2ANY for the I2C communication to configure the part to enable more connection. I consider the internal switches are FETs with low resistance. The I2C communication was finally successful, and I can read/write without issue (no NACK feedback). However, I used a multimeter to probe the two sides of the connection, for example between SDA and SD0. There is still high impedance connection. Is there any way to figure out if I have successfully connected SDA and SD0? I wrote 0x07 to the device, and I do not know if there is any problem with the communication. Thanks!