Part Number: HD3SS3220
Hi Sir
- we use Type-C positive inserted (Tx1/RX1), Type-C speed is USB 3.0 (100MB),
measure HD3SS3220I CC1voltage is 0.42V, CC2voltage is 4.75V
- reverse inserted (Tx2/Rx2) Type-C speed just have USB 2.0(36MB),
measured HD3SS3220I CC1voltage is 4.75V, CC2voltage is 0.42V
we can find CC1 and CC2 have changed depend on cable flippable, but reversed inserted data speed just USB 2.0, we fill Mux seems have no switched,
May you have advise us how can we check if IC work or not, or how can we debug it?
Bogey