This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822I: Question bout register typo and internal circuit

Guru 19685 points

Part Number: DP83822I
Other Parts Discussed in Thread: DP83822H, DP83848I, TLK105L, TLK105, TLK106, TLK106L

Please let me know about two points below for DP83822I (or DP83822H) function.

①About datasheet page-65, default value is described "101 1111 1111" and "0x5EE", which is correct?

②Basically, Are DPxxxxx series based on the same internal circuit?

 For example, are DP83822I and DP83867's 100 Base-T internal block is the same process? (in addition, ADC/DAC block, etc)

 If Yes, is old Ether PHY series (DP83848I) the same process,too?  

Best regards,

Satoshi

  • Hi Satoshi,

    0x5EEh is correct. The bit field is incorrect. Thank you for pointing this out.

    DP83822 and DP83867 are same process but do not have similar blocks.
    The DP83822 is pin-to-pin compatible to the TLK105, TLK105L, TLK106 and TLK106L PHYs so this device is a current mode line driver design.
    The DP83867 is a voltage mode device.

    The DP83848 is an older process than the DP83822 and DP83867, which is why the DP83848 has higher current than the other two devices.

    Kind regards,
    Ross