Part Number: TMDS181
Other Parts Discussed in Thread: TCA9617B
In my application, there is a TMDS181 in the Tx and Rx units. When the Tx was operating standalone, the SCL/SDA lines worked normally. The Rx also worked normally when operating standalone.
However, when the Tx was connected to the Rx per the application setup below, the video generator was not able to read the EDID reliably from the monitor. At times the video generator experienced a DDC bus timeout when trying to read the EDID.
Application setup:
Video generator => (Tx) TMDS181 => cable => (Rx) TMDS181 => Monitor
Tx TMDS181 configuration: Lane swap enabled, Polarity swap enabled, Retimer mode across full range 250 Mbps to 6 Gbps; Active DDC block bypassed per Figure 35 of datasheet.
Rx TMDS181 configuration: Lane swap enabled, Polarity swap enabled, Retimer mode across full range 250 Mbps to 6 Gbps; connected to Active DDC block.
Should the SCL/SDA lines be able to operate normally in this application?