Hi,
I am using "SN65HVD485ED" RS-485 chip. The termination resistor value is 120E. Pull to pin A is 1.2K & pull down to pin B is 1.2K. I am using Modbus poll software to generate the query. I have connected three device on the bus. I am sending query to only one device after every 3 sec. The response received from end device having 20% error from the total query sent. Means if Modbus poll software sent 100 query, i am getting response for all with 20 having "Checksum error" , "Insufficient byte received" such a error.
Can anybody help me out that what is going wrong?
Thanks