Part Number: SN65HVD234
I am having issues with the CAN transceiver in the title. I have attached a screenshot of the input to the D line and the output of the CAN_L line. We have checked that the chip is soldered the right way and that the EN, Vcc are connected directly to our 3.3V rail and the Rs and ground are connected directly to ground. The output of the chip is connected to a bus with 60 ohms differential impedance and low capacitance (1m cable). We have tried multiple chips.
This image is the input to the D pin of the chip,.
This is the output. The rate should be 500kb/s
This is the output at CAN_L with a ~50kb/s signal. Even at these speeds it still exhibits slow transition times.
Thank you.