Part Number: SN65HVD62
I'm using the SYNCOUT line from one SN65HVD62 to drive a second SN65HVD62. Per the EVM datasheet, the SYNCOUT has a 1K pull-up resistor to Vcc and the signal is connected to the slave device through a 10K resistor. The XTAL2 input of the slave deice is grounded. When I observe the SYNCOUT prior to the series 10K resistor, the signal swings from GND to Vcc (5VDC). At the XTAL1 input of the slave device (after the 10K resistor), the signal is about 1.1VPk-Pk and 1.5VDC off of ground.
The datasheet implies that a XTAL1 logic HI has to be a minimum of 0.7Vcc. Should the XTAL1 input attenuate the signal this much? Also, is the 10K series resistor necessary?
Thank you, Doane.