Part Number: DS25BR100
Other Parts Discussed in Thread: DS90CR287,
Hi There,
Our customer is using DS25BR100 as a buffer to transmit LVDS to a frame grabber, the frame grabber doesn't recognize the signals. However, if there is a 3rd party repeater, which consists of a SerDes DS90CR288 and DS90CR287, in between, the frame grabber then can recognize LVDS signals. The following is the signals captured. It's obvious that the magnitude of the signals without the repeater is higher. Is there anything we can look into?
Thank you
without the repeater from 3rd party
With the repeater in between DS25BR100 and the frame grabber
regards,
Kevin