Part Number: DP83867IR
Hi,
One of my customers is using the Xilinx SoC to interface with our phy. The 1.8V logic level from the SoC has a max value of 0.45V for the logic 0. In case of our device, the maximum level suggested in the datasheet for a 1.8V logic low is 0.2 x VDDIO(i.e. 0.2 x 1.8) = 0.36V
Would this 0.45V level cause an issue for the phy?