Part Number: TLK2711-SP
Hello,
We are using a couple of TLK2711A, each one of them functions as transmitter and receiver.
The clock is 100MHz
We are sending 0xBC 0xC5 with the toggling of the TKLSB only and the frame size is 2016 bytes.
Connecting the Tx chip to the Rx chip on the same board, it works without errors
When the Tx and the Rx are on different boards (clocks), we losing byte every 1 sec.
Please advice
Thanks,
Yohay