This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS125DF410: DS125DF410 - What is meaning of HEO and VEO from 0x27, 0x28 register?

Part Number: DS125DF410


Hi Team,

DS125DF410 support eye monitoring feature thru 0x27 and 0x28 register.
If customer want to check channel 0 eye-diagram, they have to write below register.

0xFF 0x04 - Read target chaneel 0
Read 0x27 - HEO value
Read 0x28 - VEO value

What is meaning of 0x27 and 0x28 register value and how can covert these value?
Thank you.

Best Regards,
Jade

  • Hi Jade,

    The VEO value must be multiplied by the Voltage range setting in register 0x29 to determine the eye height in mV.

    For setting 00'b the eye opening is 3.125mV per LSB in the HEO register.

    Setting 01'b=6.25mV,  Setting 10'b=9.375mV, and Setting 11'b=12.5mV 

    The HEO value is multiplied by 1/64 to determine the horizontal eye opening in UI.

    Regards,

    Lee