Other Parts Discussed in Thread: TFP401
When used with the following configuration, the resolution output from TFP410 will be 960 x 1080p60Hz?
24-bit Single-edge (1-pixel/clock) mode is 19202 x 1080p60Hz output.
1920x1080p60Hz -> TFP401 -> TFP410 -> 960 x 1080p60Hz
TFP410 :
ISEL: Low (I2C off)
BSEL: Low (12-bit Dual-edge)
DSEL: Low ((VREF = DVDD), DSEL is a don’t care)
EDGE: Hi (Rising edge)
DKEN: Low (Skew disabled, but driving this high causes no change)
DK1-3: Floating
VREF: Hi (VDD = 3.3V) Same VDD as the video source logic outputs
TFP401 :
OCK_INV: Hi (rising edge)
PIXS: Hi ( 2-pixel/clock)
DFO: Low (ODCK runs continuously)
STAG: Hi (Normal simultaneous even/odd pixel output)
ST: Hi (: High drive strength)