Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HD3SS215: What's differences between TS3DV642 and HD3SS215

Part Number: HD3SS215
Other Parts Discussed in Thread: TS3DV642,

Dear Sir,

TS3DV642 and HD3SS215 are 2:1/1:2 Differential Switch
How to choose?
HD3SS215 are there any function better than TS3DV642?

  • Hi Vincet,

    This is a summary of the main differences between HD3SS215 and TS3DV642.

    Part #

    HD3SS215

    TS3DV642

    # of Pins/Balls

    50/56

    42 pin

    Package Size

    5mm x 5mm
    8mm x 8mm

    9mm x 3.5mm

    -3dB bandwidth

    7 GHz

    PortA 6.9 GHz       PortB 7.5 GHz

    Dynamic Char Freq*

    3GHz

    1.7GHz

    Cross Talk (dB)

    ZQE -35dB      RTQ -35dB

    -40 dB

    Isolation (dB)

    ZQE -22dB      RTQ -16dB

    -23 dB

    Insertion Loss (dB)

    ZQE -1.6dB      RTQ -2.4dB

    PortA -0.75 dB        PortB -1.0 dB

    Return Loss (dB)

    ZQE -12dB      RTQ -13dB

    -15.9 dB

    Power (Active)

    <9mW typ

    180uW typ

    Power (Low)

    < 30uW typ

    < 30uW typ

    VCC

    3.3V

    2.6V to 4.5V

    ESD (HBM)

    1.5kV

    2kV

    Temp Range (˚C)

    0 to 70  & -40 to 85

    -40 to 85

    Regards