Part Number: LMH1218
Hi @ All,
We're going to use the LMH1218 in one of our camera designs. We want to use IN0(+/-) and OUT0 for 75Ohm SDI output.
After considering the datasheet I'm unsure what to to with the unused input IN1(+/-) and output OUT1(+/-). I would leave the output open (unconnected) and disable it (Reg_0x31[1:0] = 0b01). Should I connect the unused input (Pin 8, 9) to GND, or are they internally biased to a proper DC-level because of the required AC-coupling?
Any advise would be nice.
Best,
Robert