Part Number: TFP410
Hi,
I have a question about TFP410PAP.
My customer are having a problem with TFP410.
In their custom board, clock input for TFP410 is 40MHz or 66.66MHz.
The input clock can be switched(40MHz or 66.66MHz).
After switchig the input clock from 40MHz to 66.66MHz during system are running,
an output clock from TFP410 will be disordered(clock frequency will be about 80MHz) a few second to several minutes later.
(After this issue occur, the output clock will return to 66.66MHz)
When this problem occur, the connected monitor will be blackout for a moment.
Have anyone heard or had same issue using TFP410?
best regards,
g.f.