This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IS: Auto-negotiation configuration, RX_CTRL strap

Part Number: DP83867IS

Hello

 

I have some questions for DP83867IS.

 

1)

There is the below description on 8.3.3.8, P30 of the datasheet(SNLS504B).

“If Auto-Negotiation is disabled by strap option Auto-Negotiation can not be reenabled”.

 

Does it mean it is impossible to reenable Auto-Negotiation by accessing BMCR register?

 

2)

Now RX_CTRL strap is open. it means RX_CTRL=Mode 1.

Then Autoneg Disable strap is N/A.

In this case, which is auto-negotiation set, enable, disable or unknown?

If not enable, is it possible to configure enable by writing BMCR register in this case?

 

Regards,

Oba

  • Hi Oba,

    1. Yes, this is correct. If auto-negotiation is disabled by strap, using BMCR to reenable auto-negotiation is not valid.

    2. If RX_CTRL is in mode 1, auto-negotiation disable = 0. That means auto-negotiation is enabled. But mode 1 is not valid on the DP83867. Please read the table note that says RX_CTRL should be in mode 3 or 4. If that cannot be done, a register setting must happen on every reset of the PHY.

    Best Regards,