This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3USB3031: Two 3:1 switch can be uses as independent switch or one set of differential switch

Part Number: TS3USB3031


Hi team,

Please advise me a question bellow.

I want to used TS3USB3031 as two independent 1:3 switch to handle two single-ended signals.
Some of switch ICs may be designed as differential switches..
I concern that the cross talk between D+ and D- signals.
Are there any data on the crosstalk between D+ and D- on nine possible switch configurations?

Mita