Part Number: DS80PCI402
Other Parts Discussed in Thread: DS50PCI402
Customer is considering DS80PCI402 for 3.125Gbps FPGA(Xilinx Kintex-7) solution.
Please let me check about five points below.
①At first, Can DS80PCI402 use for 3.125Gbps FPGA connection?
If yes,
②Is there careful point for register map and external component?
For example, register is set to 2.5Gbps / 5Gbps / 8Gbps by 0x11 (datasheet P29).
If in the case of 3.125Gbps, is 0x11 set 5Gbps (Gen-2) correct?
Is there point of change?
③About use case of 3.125Gbps, Is there possibility of spec down the DS80PCI402?
④When set to 5Gbps, is there frequency (or speed) border of EQ:0dB or not?
⑤If DS80PCI402 can't use 3.125Gbps, is there recommend device?
【Background】
・Block diagram image is below.
・Customer is carefully whether DS80PCI402 can use certainly, for the reasons of customer application.
Best regards,
Satoshi