Part Number: DP83822I
Hi,
we are using a DP83822I with a ST Controller. When we set the PHY to 10Base-Tx there are no Problems and we can use a TCP server loop back example from ST.
When we select 100Base-Tx or Autonegaotiation the PHY can not get a stable link to the ethernet switch. The link cycles with up time for about 500ms and down time for about 1s.
When we take a look at the registers 0x10 the bit 1 (speed status) changes from 0 to 1 and back. With automdix we get the following Register entries:
Here is the schematic of the DP83822I interface:
We have done some measurement of the signals between the eternet inductor and the PHY showing a link puls, communication in autonegatiation mode and a autonegotiation paket:
Has someone the same problems with the PHY?
Regards Mario