We are currently interested in using the DP83849IF for a media converter application using SFP modules.
We have in our possession an evaluation board for the DP83849I. My question is, can this board be converted to work with the 83849IF IC if the IC is removed from the evaluation board and replaced with a DP83489IF and adapting an SFP connector to the Port B fiber module footprint? If this can be done, are there any other component changes which would have to be done to the board besides connecting the optical interface and disconnecting the copper interface on Port B?