Part Number: DS90UB948-Q1
Dear Team,
My customer is using DS90UB947 and DS90UB948 on their board design.
They found that D_GPIO of UB948 drop suddenly then goes high without any reason. And then the panel will blink. But 947 D_GPIO1 is always high.
This issue sometimes happen, but sometimes it didn't happen all the morning.
My customer capture the issue by video as below.
(The upside line is 948 D_GPIO1, and the downside line is 947 D_GPIO1)
Here is the register of 947 and 948.
947 register:
ADD DATA
0x17 0x9E
948 register:
ADD DATA
0x34 0x02
0x1D 0x05
0x1E 0x55
0x1F 0x05
Another question of 947 and 948,
My customer choose the internal timing source and spec HD 1080p 60 Hz to generate the test pattern to panel.
But why the status shows that it only has 40 frame/Second? Please see below figure.
We try to change the timing source to external source, then the status shows 60 frame/Second normally.
Therefore, could you help to provide the spec of internal clock to us?