Part Number: DP83867E
Hi Team,
I have question about DP83867 need you help ,thanks.
1. I don’t use SGMII mode.
Can I use Rhi=4kohm and Rlow=10kohm option on RX_D0~RX_D3?
Then,
I want to set”0x03:address for RGMII mode.
RX_D0=pull hi, RX_D1=pull hi, RX_D2=pull low, RX_D3=pull low. OK?
2. For the information, it seems LED0 is main indicates. Right?
If so, I will modify that. LED1 and LED2 are floating .OK?
3. I don’t know where we can use GPIO. Those pins are floating. OK?
4. How about JTAG? Do we need that?