Other Parts Discussed in Thread: AM4376
Hi,
I have AM4376 custom board with DP83849IVS.
link is up but not getting the ip [manually set the ip]
But unable to ping to any other ip, only 127.0.0.1 is working
Please help to resolve the issue
=> mii info
PHY 0x02: OUI = 0x80017, Model = 0x0A, Rev = 0x02, 100baseT, FDX
PHY 0x03: OUI = 0x80017, Model = 0x0A, Rev = 0x02, 100baseT, FDX
=> mii dump 0
Error reading from the PHY addr=00 reg=00
=> mii dump 1
Error reading from the PHY addr=01 reg=00
=> mii dump 2
0. (2100) -- PHY control register --
(8000:0000) 0.15 = 0 reset
(4000:0000) 0.14 = 0 loopback
(2040:2000) 0. 6,13 = b01 speed selection = 100 Mbps
(1000:0000) 0.12 = 0 A/N enable
(0800:0000) 0.11 = 0 power-down
(0400:0000) 0.10 = 0 isolate
(0200:0000) 0. 9 = 0 restart A/N
(0100:0100) 0. 8 = 1 duplex = full
(0080:0000) 0. 7 = 0 collision test enable
(003f:0000) 0. 5- 0 = 0 (reserved)
=> mii dump 3
0. (2100) -- PHY control register --
(8000:0000) 0.15 = 0 reset
(4000:0000) 0.14 = 0 loopback
(2040:2000) 0. 6,13 = b01 speed selection = 100 Mbps
(1000:0000) 0.12 = 0 A/N enable
(0800:0000) 0.11 = 0 power-down
(0400:0000) 0.10 = 0 isolate
(0200:0000) 0. 9 = 0 restart A/N
(0100:0100) 0. 8 = 1 duplex = full
(0080:0000) 0. 7 = 0 collision test enable
(003f:0000) 0. 5- 0 = 0 (reserved)
=> mdio list
ethernet@4a100000:
minicom log :
[ 44.945955] net eth0: initializing cpsw version 1.15 (0)
[ 44.951628] net eth0: initialized cpsw ale version 1.4
[ 45.095880] net eth0: ALE Table size 1024
[ 45.176498] net eth0: phy found : id is : 0x20005ca2
[ 45.479818] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
cpsw 4a100000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[ 48.218265] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
root@am437x-evm:~# ifconfig
eth0 Link encap:Ethernet HWaddr C4:BE:84:CB:12:32
inet6 addr: fe80::c6be:84ff:fecb:1232%132688/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:43 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:7667 (7.4 KiB)
Interrupt:143
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1%132688/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:323 errors:0 dropped:0 overruns:0 frame:0
TX packets:323 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1
RX bytes:24632 (24.0 KiB) TX bytes:24632 (24.0 KiB)
root@am437x-evm:~# ethtool eth0
Settings for eth0:
Supported ports: [ TP MII ]
Supported link modes: 10baseT/Half 10baseT/Full
100baseT/Half 100baseT/Full
Supported pause frame use: No
Supports auto-negotiation: Yes
Advertised link modes: 10baseT/Half 10baseT/Full
100baseT/Half 100baseT/Full
Advertised pause frame use: No
Advertised auto-negotiation: Yes
Link partner advertised link modes: 10baseT/Half 10baseT/Full
100baseT/Half 100baseT/Full
Link partner advertised pause frame use: Symmetric Receive-only
Link partner advertised auto-negotiation: Yes
Speed: 100Mb/s
Duplex: Full
Port: MII
PHYAD: 3
Transceiver: external
Auto-negotiation: on
Supports Wake-on: d
Wake-on: d
Current message level: 0x00000000 (0)
Link detected: yes
Device tree changes:
&cpsw_emac0 {
phy_id = <&davinci_mdio>, <3>;
phy-mode = "gmii";
};
Thanks in advance