This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

xio2001: Vss connections for PNP PowerPAD HTQFP Package

Part Number: XIO2001
Other Parts Discussed in Thread: XIO2001

In the data sheet for XIO2001 (SCPS212I –MAY 2009–REVISED JANUARY 2016) the pin specification table under section 5.2 has is no connection specified for Vss on the PNP package. 

The data sheet contains no specification that I can find of what electrical connection there is to the pad on the bottom of the package. The data sheet should specify that connection. 

I assume that the Vss connection is made through the Pad on the bottom of the package, but I cannot know that without a specification. 

Can someone from TI confirm that the XIO2001PNP (XIO2001IPNP) part has Vss connected to the pad on the bottom of the package?

Ian Lewis

www.mstarlabs.com