Part Number: TPS2546
Hi Team
may I get your confirm ?
[1] if I set one of the below two settings marked by the red [1] and [2], what is the OUT Discharge duration applied at Load detected, TYP 2 sec or TYP 310 msec ?
[2] if I set one of the below two settings marked by the red [1] and [2], and 1.2V Charging Scheme is used,
the 2A Charging current is supported ?
i just want to know 2A Fast Charging way...