Part Number: TPS65982-EVM
Other Parts Discussed in Thread: TPS65982
Hi,
I am working on a project that needs to send VDMs, but when I try to send one using the Host Interface GUI I get the following error message: "Error -> Task Status: 3(REJECT_CMD).
This is with the recovery mode (tps65982_evm_flash_image.bin) firmware on the device. Is there a setting somewhere that needs to be changed so that the VDMs command is allowed?
I tried modifying the code in the DRP Host Advanced template ( uncommented the 'VDMs' command from the cmdReportDict and the cmdTaskReportDict dictionaries) but still got the same error. Maybe a different template would be a better fit for sending a VDM?
Thanks,
Ross