Part Number: DP83867E
Hi team,
The customer is using DP83867. The attach is his schematic. There are some questions for the schematic as below:
Q1: The datasheet shows"For SGMII Mode 4 strap, TI recommends using Rhi = 4 kΩ and Rlo = 10 kΩ on RX_D0 and RX_D1 , RX_D2 and
RX_D3."
But the customer uses the RGMII mode. Can the customer use Rhi=4kohm and Rlow=10kohm option on RX_D0~RX_D3,
that is RX_D0=pull hi, RX_D1=pull hi, RX_D2=pull low, RX_D3=pull low. OK?
Q2: How to deal with the GPIO_0 pin and GPIO_1 pin? floating?
Q3: Can only use LED_0 pin,not use LED_1pin and LED_2 pin in the RGMII mode ? If it is ok, then LED_1pin and LED_2 pin can be floating?
Q4: Are the JTAG pins pins needed to use? If not ,then the JTAG pins can be floating?
Q5: There are only the DP83867ERGZ-R-EVM Altium file on our website. The customer needs the PADS file or the Allegro file.
Do we have the PADS file or the Allegro file for the DP83867ERGZ-R-EVM?
Best Wishes,
Mickey Zhang
Asia Customer Support Center
Texas Instruments