Part Number: DP83848Q-Q1
Hi,
I have a question the operation when 3.3V power supply drops to 2.5V.
For example, internal reset is applied, power down, registers are held but not output etc.
I would like to know each situations when only IOVDD dropped, when only AVDD dropped.
In order to think about the configuration of the power supply, I need to know the above conditions.
Please let me know the threshold voltage at which the register is held and the threshold voltage at which it shuts down.
Best regards,
Tomoaki Yoshida