Part Number: TCAN337
Hi,
I am using multiple TCAN337 ICs for a CAN bus with many nodes in my design. Every once in a while I notice the CAN transceivers stop working. Whenever this occurs, I can measure a low impedance (close to 0 ohms) between the CAN_H pin and ground and the CAN_L pin and ground. The IC always breaks in this manner regardless of the CAN node. After various unsuccessful attempts to recreate this failure mode, the suspicion turned to ESD as each CAN node is exposed outside of it's chassis through a connector. I added ESD protection diodes and did not see the problem for 3 weeks after seeing the problem a few times a day prior to the ESD diodes. However, the problem occurred again after adding ESD protection. Are there any vulnerabilities this particular IC has that would lead to this behavior?
Thanks,
Josh