Part Number: TRS3253E
Hi team,
The customer is using TRS3253E. He would like to test two parameters. One is |tPHL – tPLH| that is in the 6.9 Switching Characteristics—Driver
of the datasheet. Another is ten and tdis that is in the 6.10 Switching Characteristics—Receiver of the datasheet.
VCC is 3.3V and C1~C4 is 0.1uF in his circuit.
(1). Test |tPHL – tPLH|:
The customer's test is as below:
The input is DIN pins. The output DOUT pins. Is this correct?
Then the test result is that |tPHL – tPLH| is 4ns.
If the customer's test is uncorrect, how to test this parameter?
For the |tPHL – tPLH| testing, I notice the Figure 4. Driver Pulse Skew of the datasheet. It is the |tPHL – tPLH| testing.
I would like to verify which pin the input is and which pin the output is when the customer tests the |tPHL – tPLH|.
(2)Test ten and tdis:
The customer's test is as below:
The input is FORCEOFF pin. The output is ROUT pin. Then the customer control the high level or the low level for the FORCEOFF pin through the software,
test the level changes of the ROUT pin. Is this correct?
Then the test result is ten=85ns;tdis=1650ns.
I notice the Figure 6. Receiver Enable and Disable Times. For Figure 6, I think the input is RIN pin and the output is ROUT pin, then FORCEOFF is connected
to GND and FORCEON is connected to GND or 3V. Is my understanding correct? I also would like to verify which pin the input is and which pin the
output is when the customer tests the ten and the tdis.
Best Wishes,
Mickey Zhang
Asia Customer Support Center
Texas Instruments