Part Number: USB-REDRIVER-EVM
it looks like the USB-REDRIVER-EVM has a dual footprint for both A plug and A receptacle. Great idea assuming there are no problems! I see the A plug on the schematic, but no mention of the A receptacle anywhere (or resistors R23-R28 which I assume are installed).
is the dual footprint functional? I wanted to make sure it wasn't intentionally removed from the manual.
are R23 - R28 just 0 ohm 0201 resistors?
Can I get the gerber files for this EVM? It looks like care was taken to not make any stubs with the dual footprint, I wanted to get a better view of how it was routed.
Thanks,
Matt