Part Number: TPS65986
Other Parts Discussed in Thread: TPS65982, HD3SS460
I am working on a USB-C design, with the TPS65986 currently penciled in, although I am willing to change to the TPS65982 if necessary.
Requirements:
- Power source 5V/3A (available through internal PP_5V0 power path on any TPS6598x device)
- Power sink 27W profile minimum (9V/3A min, 15V/3A max) (available through internal PP_HV on any TPS6598x device)
- Dual role data port supporting USB 2.0, USB3.0 + 1-lane DisplayPort, or 2-lanes DisplayPort only alternate mode (using HD3SS460 in slightly non-standard config for high-speed signal mux)
- Desirable: Support Debug Accessory Mode with pass-through of 2-4 internal signals (console UART etc.) for factory test procedure.
Since my power requirements can be met using the internal power paths on any part, and I don't require thunderbolt support, I originally thought that the TPS65986 would be appropriate. However, I am confused by the GPIO and debug configurations:
-The pinout documentation of both parts lists GPIO0-8, RESETZ, BUSPOWERZ, MRESET, and DEBUG1-4, but in the pinout table refers to all of these pins as GPIOs. Additionally, the TPS6598x Application Customization Tool (version 3.4) has a section under Shared Device Settings -> GPIO Event Map where it appears that these I/O are all flexible. However, it appears that GPIO4 and 5 are specifically defined to relate to displayport HPD.
Question 1: Which GPIO pins have specific definitions that cannot be changed by software configuration?
-The TPS65986 mentions the port data multiplexer, debug accessory mode, and has 4 pins labelled DEBUG1-4, however in the datasheet on page 47 it does not actually show the DEBUG pins as capable of routing through the mux in debug accessory mode. Moreover, the application configuration tool doesn't show any configuration for this mode. The TPS65982 does show DEBUG1-4 (as well as two additional pins, LSX) as routing through the mux (datasheet page 52) but provides little additional information on the configuration of debug accessory mode. The application configuration tool also does not show any configuration options for this.
Question 2: Does the TPS65986 support pass-through of system signals using debug accessory mode? If so how is it configured? If not, does the TPS65982 support this and how is it configured? Would there be other design changes required to move from -6 to -2?
Question 3: Can the TPS6598x devices drive their GPIOs such that the HD3SS460 AMSEL and EN pins can be driven to the mid level / floated? My current mode mapping is for USB 3 + 1-lane DP [AMSEL=H, EN=H] and for 2-lane DP only [AMSEL=M, EN=M]. This configuration is because my host processor has two transceiver channels available, one of which is DisplayPort lane 0 and the other of which is either USB3 or DisplayPort lane 1.
Thanks!