Part Number: DP83849IF
Hello,
Following the reference design (DP83849IFVS-EVK) I put the DP83849IF in one of my board with the aim of use it as a Media converter R45 to fiber.
I had some issues because the datasheet isn't really clear about the loopback of RMII signals: I think that there must be a cable between the J9 and J14 connectors.
Anyway, I tried to tie signals TX from port A to RX of port B and viceversa (port A is copper, port B is Fiber).
I read that, for RMII, it is sufficient to tie RXD[1:0] to TXD[1:0] (A to B, B to A), and RX_DV to TX_EN, with this connection pull up to VCC by a 2.2Kohm resistance.
The clock is the system clock and it's the same for the 2 ports (a 50 MHz oscillator).
The conversion doesn't happen.
Can you suggest me if there is something that I miss? Can you suggest me some way to investigate about the point where the chain interrupts itself?
Thank you