Part Number: ISO5452-Q1
Other Parts Discussed in Thread: ISO5452, UCC21520
Hello,
For the ISO5452, can I drive the RESET pin with an active low signal to disable the outputs? I have windowed comparators that trigger for overcurrent events on the 3 phases and then another to trigger for a overload on the DC bus. I want to feed the output of those comparators to a logic gate where the output will bypass the processor and go directly to the gate driver to open the IGBTs in case of a overcurrent or overload event. The reason for this is to reduce propagation delays and latency.
I see the UCC21520 has a DISABLE pin. That is exactly what I want. Can the RESET pin on the ISO5452 do what the DISABLE pin does?
Thanks
Jason