This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB914A-Q1: ID[x]:10K Ohm register

Part Number: DS90UB914A-Q1


Dear support team;

The slave address is 0x60(7bit).

In this case, Rdi[1] and Rdo[0] is 0 ohm.

And, I want to connect ground whith out 10k ohm registers.

Is this all right?

Best regards

 M.Sugiyama