This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848K: Question about DP83848K circuit (termination, short distance, impedance)

Guru 19685 points

Part Number: DP83848K

Please let me know about three points below for DP83848K.

①About datasheet page-65(Figure 7-2), is resistor value required 49.9Ω only?

 If in the condition of RJ-45 side, is resistor value change to 47Ω, no problem? 

②Is there information for impedance control?

③If there performance data for "very" short distance transmission?

 For example, ~50cm distance.

Best regards,

Satoshi