This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1042HG: TCAN1042HG

Expert 1070 points

Part Number: TCAN1042HG

Hello,

Can anyone advise me if  TCAN1042HG has similar characteristics as TJA1043TK (NXP) ,if not maybe other TI CAN recommanded.

Thanks

  • Hi Hen,

    The devices are similar in that they are both CAN transceivers (convert logic-level IO from a CAN controller to differential CAN bus signals), but the TJA1043 has a few extra features that allow for lower system-level current consumption (i.e., the ability for the device to run directly off a battery in sleep mode and then wake up an external DC/DC regulator via a high-voltage control output when CAN data is detected on the bus).

    If you send me an email at m-robertson at ti dot com I can give you more information on future CAN devices from TI.

    Max