Other Parts Discussed in Thread: LMH0344, LMH0356, LMH0318, LMH0324
Hi,
Can you suggest me the best possible solution w.r.t. cost and area for a 2:1 Mux for SD/HD/3G-SDI interface?
FYI, the 2 input SDI signals are provided from an external source over a BNC connector and output SDI signal is connected to an SDI receiver on board.
I see that LMH0356 (Mux) along with LMH0344 (Equalizer) meets the above requirements.
Is there any other recommended solution to save on cost and area based on above requirements? Can a 2:1 LVDS Mux be used instead of LMH0356? If yes, please suggest a suitable device.
Regards,
Raja