Part Number: LM1881
Hi,
From the datasheet it seems that the Vcc voltage at 8th pin of LM1881 IC ranges from 5 to 12V.
We can understand 12V is the maximum acceptable voltage at this pin.
What is the minimum acceptable voltage at this pin? Is it 5V?
Can the board function normally, say when Vcc drops to 4.9V.
Please inform the exact minimum Vcc voltage below which the IC LM1881 ceases to function.
Please clarify on this ASAP.
Thanks a lot in advance.