Part Number: SN75188
Other Parts Discussed in Thread: SN75189
I am trying to design a circuit which has an input like an +-7V square wave and changing it to a 1V peak-to-peak square wave (+-0.5V or 0-1V not important) with saving its shape of signal. Circuit will work double-sided (1V peak-to-peak signal can be converted to +-7V also). I have to design this cirucit TI SN75188 Driver (for +-7V to 1V peak-to-peak) and TI SN75189 Receiver (for 1V peak-to-peak to +-7V). Usage of these ICs is a restriction, so i can not use any opmap to make this circuit. Do you have an idea related to how i can obtain this levels using these ICs? Do i need anything else to get my specifications? The frequency of +-7V signal is 16kbit/s. This is a similar signal to RS-232 but not it actually.
Driver has +-9V and receiver has +5V supply voltages. I am considering that taken this voltages from a transformer and full-wave bridge rectifier and proper regulators.
If you share your ideas i will be happy. Thank you so much.