Part Number: TS3USB221E
Dear, Sir.
My customer is considering to apply TS3USB221E under the condioon as ;
1) VCC is applied from external 3.0V.
2) /OE is controled by 1.8V bus line. It will be pulled up by 2.2kOHM resister.
3) During the start-up, 1.8V applied first, then 3.0V VCC will be applied.
I would like to make sure followings.
1. I would like to make sure /OE input threshold. I wonder VIH & VIL (defined on page4) would
correspond to these?
2. Data sheet 9.2.1 Design Requirements is defined the recommendation /OE to be pulled up
to VCC. Is it no problem that /OE will be pulled to another voltage source(1.8V) not VCC?
3. If above #2 was OK, Please recommend the proper value as pull-up resistor.
4. If you find the remarkable point on 1) to 3) condition especiaaly start-up, Please let us know.
Best Regards,
H. Sakai