Part Number: TUSB8020B
Other Parts Discussed in Thread: TUSB8040, TUSB8041
I have an I2C EEPROM connected to a TUSB8020B. With an unprogrammed EEPROM the hub enters a sate where it is waiting to program the EEPROM. I used the TOOL to program the EEPROM, but I want to change a parameter. But now since 00h is set to 55h, the chip does not go into the waiting to be programmed mode and the TOOL will not connect.
So, how do I re-program the EEPROM once 00h is already at 55h?
Thanks,
John S.