Part Number: TPS65981
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS65981
Hi Manikandan,
You can use the internal ADC to read the SINK current on PP_HV using the TPS6598x Utilities GUI by using the ADCs command in the Command List tab. The ADCs channels are listed there with "Thermal_Sense" as channel 0. The channel for I_PP_HV would be channel 5.
The TPS65981 will boot using a SPI Flash chip connected to it on the PCB. After the device has booted, it is possible to reconfigure some registers using the Host Interface commands over I2C. It does not support programming through SWD.
Thank you,
Eric
Thank you, Eric. It seems we require USB-I2C host adaptor to work on it with our real time hardware and we order the same to get started with it.
We would like to explore the TPS65981 programming through SWD interface. Please suggest us with the appropriate Debugger kit from TI if any.
Likely, if we manually reset the TPS65981 (through MRESET pin) would it reboots and initiates the PD communication on CC lines? If I intend to reset the USB-C controller TPS65981 runtime on USB PD Sink Only device, it may result in power cycling. Is this understanding correct?
Regards,
Manikandan M V
Thank you, Eric.
Just to be more clear, we tie BUSPOWERZ to 3.3V and the TPS65981 loads our custom application setting. We define sink PDO's 5V/2A & 5V/3A pass from VBUS to PP_HV in binary. Under such case, TPS65981 pass 5V power only if the configured sink PDO's are set? It won't pass nominal 5V/0.9A or different unconfigured sink PDO's are set on PD communication. Is this understanding correct?
Our target is passing only 5V/2A and 5V/3A sink PDOs from VBUS to PP_HV path. Hope I'm clear.
Thank you,
Manikandan M V
Hi Eric,
Okay, thank you. Please let us know your email id for sharing Schematics and Layout review.
Could you please share the reference manual for the commands found on TPS6598x Host Interface Tools GUI if any?
Regards,
Manikandan M V
Hi Eric,
I'm expecting your ping with the email address for sharing design review.
Also, I'm working on configuring the PD profiles as discussed above. I have configured 5V/2A sink profile using Application Customization tool and generated a .BIN (Low-Region only & Low-Region and Full Flash Image file types). Then, loaded this .BIN file into the TPS65983 Evaluation Module using Cheetah Flash Programmer. However, the 5V from VBUS is not passed to PP_HV while powering up using Google Pixel Charger Adaptor which is PD compliant upto 18W. Further probed on CC lines and observed some data flow activity on CC line. Sorry, I'm not sure whether I'm missing any measures.
Thinking to execute our Board Bring-up as to generate a 5V/2A sink PD profile .BIN file and load them into the SPI Flash memory using Cheetah Flash Programmer. Could you please support us with an appropriate .BIN file and its process flow document?
Regards,
Manikandan M V