Part Number: DP83848I
Looking at using the DP83848I with the KSZ8895 Ethernet switch with a transformerless connection on two of the switch outputs. In one case, the PHY to PHY connection is about 3.5 inches on the same board. Second connection is about 9 inches. Both will be capacitively coupled.
Application Note AN1519 provides information on forming a transformerless connection with the DP83848 PHY so this seems possible. We have a few questions:
1. Does TI have any experience with a transformerless connection to the KSZ8895? I did see another forum post related to a transformerless connection between these two devices and it appears to be OK if run at 100 Mb/s Full duplex mode.
2. Need the PHY to come up in the proper mode from strapped settings. I found a forum post on the DP83822 where it seemed a reserved register bit needed to be changed to output MLT-3 waveform. Does this apply to the DP83848I?
3. Also saw this forum post about the DP838117 having issues generating MLT-3 waveform without a transformer. Just want to verify the DP83848I will not have this issue.